Need It Fast
   
Home Applications Automotive Engine Dynamometer

Engine Dynamometer

Internal combustion engines are by far the most common power source for land vehicles. From a 2-stroke motor in a lawn mower, to a V-8 stock car engine, horsepower and torque are the bench marks of engine performance. Engine manufacture's and aftermarket suppliers use an engine dynamometer (dyno for short) to accurately measure an engines performance. An engine dyno isolates an engine’s power output to help quantify its overall performance, applying a load directly to the engine and utilizing a load cell to measure the torque absorbed by the loading mechanism. Horsepower is then calculated using the torque and RPM of the engine.

Learn how this was accomplished using a Model SSMF Fatigue Rated S-Type Load Cell and a CSC Environmentally Sealed Signal Conditioner.

Download the Application Note below.

 Engine Dynamometer App Note.pdf