Need It Fast
   
Home Applications Automotive Pedal Force Testing

Pedal Force Testing

Pedal Force Testing Application

To meet certain vehicle safety protocols, pedal force must be measured and recorded. In order to quantify the quality of the braking system, the relationship between pedal force and braking force at the axle must be ascertained, either during an on-road stopping test or in a simulated indoor environment with a dynamometer, where brake force can be measured.

Learn how this is accomplished using an Interface Model BPL Brake Pedal Load Cell along with the Model WTS.

Download the Application Note below.

 Pedal Force Testing App Note.pdf