Hydraulic fracturing is known in the energy sector as fracking. It is a process used for extracting oil and natural gas from underground. With natural gas consumption in the United States reaching a new record in 2024, methods to meet the demands require sensor-based solutions safely and efficiently.
Hydraulic fracturing is a means to expedite natural gas production. This method involves injecting a high-pressure fluid, often a mix of water, chemicals, and proppants, into the rock to create fractures. Proppant is a granular material like sand or ceramic beads injected into oil or gas wells at high pressure to hold open fractures in the rock formation, allowing for the extraction of energy sources.
As a supplier of choice in the energy sector, our load cells are integrated into the pumping systems, tension monitoring equipment, downhole simulators, wireline equipment, and wells.
Concerning hydraulic fracturing, Interface force measurement products help monitor the precise amount of proppant being pumped into the well. Interface sensor technologies are commonly used in hydraulic fracturing and proppant applications to measure the force or pressure exerted during fracking accurately.
We have developed standard and engineered-to-order solutions for these environments using our experience, technologies, and proprietary strain-gaged solutions specifically for downhole applications.
Examples of Interface Products for Hydraulic Fracturing
- Interface Pressure Compensated Downhole Cell Model (IPCD) is pressure compensated up to 20,000 PSI, temperature compensated up to 350°F. It is superior to hydraulically compensated wet load cells, which have a short life expectancy and high operating costs
- Axial Force Pressure (AFP) tension and compression load cell and a pressure transducer with 2 discrete Wheatstone bridges for output utilize a matrix conversion process to determine force and pressure.
- Custom Load Pins in various sizes and capacities to work within fracturing equipment.
Load cells have precise measurement capabilities necessary for maintaining optimal fracking conditions. Overloading or underloading the well with proppant can result in suboptimal fracturing, compromising well productivity, or even causing structural damage to the wellbore.
Hydraulic Fracturing Applications Using Interface Sensor Technologies
- Downhole Tension Monitoring
- Tool Strings
- Wireline Equipment Monitoring
- Proppant Injection Monitoring
- Fracturing Pressure Monitoring
- Proppant Transport
- Proppant Storage Silos
- Proppant Testing and Quality Control
- Wellbore Stability Monitoring
- Pump Tools
Interface load cells are used in equipment for measuring factors that impact safety and environmental sustainability in hydraulic fracturing operations. For example, by accurately measuring forces exerted during proppant handling, load cells may lessen the risk of equipment failure or unintended environmental impacts.
Interface’s load cells and instrumentation provide precision, reliability, and real-time monitoring capabilities. The data we provide using our force sensors also helps evaluate the effectiveness of the hydraulic fracturing operation, thus optimizing future procedures for maximum output.
Mining for Rare Earths and Minerals Using Load Cells and Torque Transducers
/in Uncategorized /by Jamie GlassInterface load cells and torque transducers are addressing challenges and empowering the mining sector as demand for rare earths and minerals rises. Driven by the demand for clean energy minerals like lithium and cobalt, these sensor technologies provide the real-time data needed to optimize operations, safeguard workers, and propel the industry toward a sustainable future.
The Importance of Load Cells in Oil and Gas
/in Blog /by Jamie GlassInterface load cells are used in many facets of oil and gas, including to ensure safe lifting, enhance equipment integrity, provide accurate measurements in field operations, and even assist with optimal storage tank management. Our energy solutions include load cells that are used on rigs, downhole projects, extraction tools, and field support systems. We offer products ideal for harsh environments, extreme temperatures, and even submersible projects. Learn about our dry cell technology and IPCD product for downhole operations.
ForceLeaders Summit Houston
/in Trade Show /by Jamie GlassInterface ForceLeaders Summit 2024 in Houston, Texas, happens May 9, 2024. Interface and T&M force measurement solution engineers and experts will share valuable tips and experiences using load cells, torque transducers, multi-axis sensors, and advanced instrumentation. Whether you are lab technician in the oil and gas industry or a product designer of robotics, we’ll have something for you. We’ll highlight sensor solutions for all industries. Register to join the technical conversation. Seating is limited.
Force Makes the Circular Economy Go Around
/in Blog /by Jamie GlassInterface load cells and instrumentation are used in different facilities and resource manufacturing processes within the circular economy. Our sensor technologies help to measure and monitor forces, loads, and weight within the tools, robotics, and machinery used to optimize resources. Our sensors are also commonly used to test new products for material strength, fatigue lifecycle, quality, and function.
Building a Clean Energy Future in Hydrogen with Force
/in Blog /by Jamie GlassInterface is a supplier of force measurement solutions for clean energy providers and equipment makers. Brian Peters writes about the dynamics of applying force testing in hydrogen energy to the Winter Edition of Global Hydrogen Review. Learn how force measurement is used in research, production, storage and testing of hydrogen sources and equipment.
Year in Review of Top Interface Solutions and Applications
/in Blog /by Jamie GlassInterface is at the forefront of innovative use cases and applications, providing quality devices worldwide to gather precision measurements. Interface unveils the top industry solutions, product use cases and applications that define force measurement in 2023.
Force Measurement Solutions for the Forestry Industry
/in Blog /by Jamie GlassInterface products are ideal for the forestry industry, whether designing heavy-duty machinery using load cells to prevent overloading or protecting operators with sensor-based alarm systems and monitoring tools. Interface sensors are used in forestry heavy equipment, forest and timber management, logging, wood product manufacturing, pulp and paper manufacturing, and recycling forest products.
Interface Measurement Solutions for the Natural Resources Industry
/in Blog /by Jamie GlassInterface offers various sensor technologies for research, development, extracting, processing, and preserving natural resources. Our load cells and instrumentation are critical in measuring and monitoring forces, loads, and weight in different processes, equipment, tools, and technologies used in the natural resources industry. The data acquired from Interface load cells provides tremendous value in innovation, R&D, and optimization.
Outlining Force Solutions for Structural Outrigging
/in Blog /by Jamie GlassInterface provides load cells and wireless technologies for structural outrigging. Force measurement sensor technologies provide high accuracy measurement of the outrigging equipment in test and actual use. The applications range from integrating sensors into outrigger equipment to using load cells for real-time monitoring of physical structures using outrigger supports. Interface load cells are used by outrigging engineers, civil engineers and heavy equipment manufacturers, oil and gas, construction industry and marine equipment companies.
Wireless Telemetry Systems 101
/in 101 Series, Blog /by Jamie GlassInterface offers a wide range of wireless telemetry products including load cells, transmitters, bases, communication modules and data acquisition systems. A wireless telemetry system enables the remote measurement and transmission of data from one location to another without the need for physical wired connections. Components in wireless telemetry systems typically include sensors, transducers, instrumentation, communication modules, transmitters, displays and printers. Learn more about Interface WTS products in our Wireless Telemetry Systems 101 overview.