Solution
Snack Weighing and Packaging Machine
A snack manufacturing brand wants to weigh the amount of their snacks that is automatically dispersed into the bags during the packaging process.
A snack manufacturing brand wants to weigh the amount of their snacks that is automatically dispersed into the bags during the packaging process. In this case, they want to weigh their potato chips being packaged. The company wants to ensure the potato chips are at the exact weight needed due to regulatory standards.
Interface’s solution is to use multiple SPI Platform Scale Load Cells, and install it to the potato multi-head weigher and packaging machine. The SPI Platform Scale Load cells are installed inside of the mount that attaches the head weigher to the packaging machine. Force results from the potato chips are read by the load cells and sent to the ISG Isolated DIN Rail Mount Signal Conditioner, where the customer is able to control the automated production from their command center.
The customer was able to determine the weight of the potato chips being distributed into their bags with highly accurate results. They also were able to control the automated production process with the provided instrumentation. They will use this same weighing method for other snacks that need to be packaged.