Solution
Claw Machine Strength
Manufacturers for claw machines need to measure the force strength of their claws. They need to see the force measurements in order to program their claws grip strength.
Manufacturers for claw machines need to measure the force strength of their claws. They need to see the force measurements in order to program their claws grip strength.
Interface’s ConvexBT Load Cells are installed on the fingers of the claw machine, each connected to WTS-AM-1E Wireless Strain Bridge Transmitter Modules. After a grip test is done, the force results are wirelessly transmitted to the customer’s computer where it can displayed, logged, and graphed when connected to the WTS-BS-6 Wireless Telemetry Dongle Base Station. It will also have supplied Log100 software.
The manufacturers for their claw machines were able to determine the strength of the claw grip, thus were able to program the strength of the claw.
Notifications