Solution
Beam Stress Test
A customer wants to conduct stress tests on their beams to determine the peak force and the linear displacement reading until the point of failure.
A customer wants to conduct stress tests on their beams to determine the peak force and the linear displacement reading until the point of failure.
Interface’s WTS 1200 Standard Precision LowProfile™ Wireless Load Cell is installed in the test rig. A hydraulic ram, with an installed LDVT sensor, pushes up onto the beam until it cracks or bends, and the WTS 1200 measures the forces. Data results are wirelessly transmitted to the WTS-BS-6 Wireless Telemetry Dongle Base Station when connected to the customer’s PC. The WTS-AM-2 Wireless Voltage Sensor Transmitter can also transmit results from the LDVT sensor using Log100 software.
Interface’s wireless telemetry system and products successfully graphed and logged the results of the beam’s peak force and linear displacement during the customer’s beam stress test.