Interface Advanced Sensors Assist in Simulating the Cosmos

The space industry is experiencing a renaissance. Commercial ventures, ambitious global government programs, and expanding research initiatives propel us toward a future where humanity’s presence extends far beyond Earth.

Interface understands the aerospace industry’s requirements as a decades-long trusted supplier of precision measurement solutions. The rapid expansion of the space economy, exploration, and research initiatives requires rigorous testing and validation of spacecraft, components, and methods. Accurate simulation of space’s extreme conditions is no longer a luxury but a necessity.

Accurate measurement is instrumental in space endeavors. Our advanced sensor technologies are designed to meet the demanding conditions of space simulation environments. Our products provide aerospace engineers and testing experts with the data-driven insights they need to ensure mission success.

Why Measurement Technologies are Essential to Space Simulation

Space simulation labs recreate the harsh realities of the cosmos on Earth, subjecting spacecraft and equipment to extreme temperatures, vacuum conditions, and intense forces. Sensors are the eyes and ears of these simulations, capturing critical data that validates designs, predicts performance, and safeguards lives.

Interface LowProfile and Mini load cells verify the structural integrity of spacecraft components. By accurately measuring forces and stresses during simulated launch and landing events, load cells ensure mechanisms can withstand the rigors of space travel.

Precise measurement of rotational force is essential for testing the performance of robotic arms, deployment mechanisms, and control systems. Interface reaction and rotary torque transducers provide the data needed to optimize these systems for reliable operation in the unforgiving space environment.

Accurate, quality measurement data is the key to success. Capturing forces and moments in multiple dimensions is vital for understanding the complex interactions during spacewalks, docking maneuvers, and robotic operations. Multi-axis sensors provide a comprehensive picture of these interactions, enabling engineers to refine designs and procedures.

TIP: Watch our Space Industry Product Review

Interface Solutions for Space Simulation Applications

Interface offers a wide range of sensor solutions tailored to the unique challenges of space simulation, from robotic arm testing for robots used in planetary sampling to simulations of satellite deployments.

Reduced Gravity Simulation Systems

Load cells and multi-axis sensors integrated into these systems accurately measure forces experienced by astronauts and equipment in microgravity environments.  A full range of natural motion for a realistic simulation of reduced gravity environments is essential for future missions to the moon, mars, asteroids, or any other celestial destination. The simulated weightlessness can train the crew to handle various microgravity activities, including walking, running, and jumping. The 1100 Ultra Precision Universal LowProfile Load Cell is installed in line with a steel support cable to measure the vertical load on the system actively. A control system, which includes the 9870 High-Speed High-Performance TEDS Ready Indicator, monitors the load cell output and continuously offloads a portion of a human or robotic payload weight during all dynamic motions. More Info: Reduced Gravity Simulation App Note

Spacewalk Simulators

Our sensors capture the forces exerted by astronauts during simulated extravehicular activities (EVAs), ensuring that training scenarios accurately reflect the challenges of working in space. To monitor and maintain the forces of the subject when the subject moves, a WSSB Welded Stainless Steel IP68 Environment Protected S-Beam load cell can be connected to the cable. This will monitor the constant force needed as someone is using the spacewalk simulator. The DMA2 DIN Rail Mount Signal Conditioner will signal the customer’s controller system. More Info: Spacewalk Simulator App Note

Space Robotic Testing

Torque transducers and multi-axis sensors are instrumental in evaluating the performance and dexterity of robotic arms and manipulators designed for tasks such as satellite repair and assembly. Autonomous robots will be tasked with repairing satellites and spacecraft while in space. Through this R&D phase, force and torque sensors are needed through any testing operations. Interface’s multi-axis sensors, such as the 6ADF Series 6-Axis DIN Flange-Type Load Cells, are popular in robotics testing. These sensors are easy to install and measure force and torque in 6-axes. It can be utilized during the testing stages for these spacecraft repair robots by monitoring the movements before they can be deployed in space. Paired with Interface’s BX8-HD44 BlueDAQ Series Data Acquisition System for Multi Axis Sensors, force feedback and torque can be displayed, graphed, and recorded for analysis. More Info: Spacecraft Repair Robot App Note

Space Vehicle and Rover Environment Testing

Interface sensors are critical in assessing the durability and performance of spacecraft and rovers under simulated launch, landing, and surface exploration conditions. A space company is designing a system to measure the wheel spin torque and force applied onto the wheels of their space rovers. They want to be able to monitor the torque measurements to see whether or not the rover is in motion or static as the motor runs. Interface suggests using the T14 Slip-Ring Shaft Style Rotary Torque Transducer, installed inside the rover’s wheel alongside the motor. To create a wireless system, the torque sensor is attached to the WTS-AM-1E Wireless Strain Bridge Transmitter Module, which will wireless transmit the sensor’s measurements to the WTS-BS-1 Handheld Display for Multiple Transmitters, Read Rover Wheel Torque Monitoring and check out the Vertical Farming for Sustainable Food Production on Earth and Beyond.

Inflatable Space Habitat with a laptop with supplied software, clevises and LP Load Pins

Habitat and Agriculture Simulators

Our sensors contribute to developing sustainable life support systems by monitoring and optimizing the performance of closed-loop agriculture and resource management technologies. Multiple clevises and LP Stainless Steel Load Pins are attached to the webbing material that creates the inflatable habitat in these space habitats. When pressure is increased within the inflatable habitat, the load pins will capture how much force the heavy-duty material will hold at specific pressures until it explodes. Read More: Inflatable Space Habitat

From Simulation to Beyond

Interface is at the forefront of sensor innovation. Our miniature, compact sensors can be integrated into tight spaces without compromising performance. They become part of the testing, simulators, and potentially for deployment beyond Earth’s atmosphere. Our extensive wireless telemetry solutions eliminate the need for cumbersome cables. Wireless and Bluetooth capabilities provide real-time data transmission from sensors in challenging environments.

As humanity’s ambitions in space continue to grow, the importance of accurate and reliable simulation will only increase. Interface is committed to providing cutting-edge sensor technologies to enable the next generation of space exploration. Our sensors are not merely tools but the key to unlocking a future where the cosmos becomes our backyard.

Additional Resources

Partnering to Shape the Future of Space Exploration

The Criticality of Thrust Measurement Testing in Aerospace

Interface Space Economy Solutions

Interface and The Race to Space