Finding the Center of Gravity
Even after more than a half-century in the force measurement industry, Interface continues to find new and innovative use cases for our precision products.
Recently, we were approached by a customer who needed help finding the center of gravity in order to optimize weight distribution and balance for a product in development. Our outstanding team here at Interface put our heads together to develop a unique testing method to help discover this critical data point.
“One of the most rewarding experiences in managing our custom solutions is learning about a new customer challenge and developing a novel solution to address it.” Ken Bishop, Director of Sales and Customer Solutions, Interface, Inc.
For this specific use case, the customer had a cylindrical tank filled with material for which they needed to find the center of gravity. Because we were able to calculate the distance of the tank, we were able to understand the weight distribution and create a test to find the center.
The center of gravity of an object is calculated when the weight of the given object is concentrated into the center of the object. This is determined by measuring the weight seen by each of the four legs. If the weight is distributed evenly, the material is in the center location. This center location can also be referred to as the origin.
Utilizing a Model 1280 Programmable Weight Indicator and Controller, which is highly customizable instrumentation for any application, we were able to write a program to achieve our goal. We then placed two Model 1211 Standard Precision LowProfile® Load Cells on each end of the rack where the tank resided, using four load cells in total. Because we knew the distance of the object and had load cells to measure the weight at both ends, we were easily able to calculate and identify the origin point on the tank. In this case, the center of gravity.
Ken noted that during his tenured career at Interface, this was the first time he and the team had been tasked with finding the center of gravity in relationship to the distance for an object. As Interface’s team thought about how to develop the custom solution, they also considered additional applications in which this information could be beneficial.
The result of this successful test and measurement application, Interface considers the center of gravity analysis as a beneficial test to optimize flight performance of an airplane. This is important when there is that instant that a plane is not flying at max capacity. There may be open seats all around you, but in order to keep weight distribution in balance, the attendants may need to limit which seats are occupied during a flight. If planes were equipped with this type of sensor technology to calculate center of gravity, they could more evenly distribute weight and ensure optimal performance. This same type of application can apply to any vehicle that moves on land, air or water with people or cargo.
SEE THE APPLICATION NOTE FOR CENTER OF GRAVITY TESTING
In the growing demands for urban mobility, unmanned vehicles and drone technologies, this type of testing application can help with vehicles, aircraft, space vehicles, boats and more with performance and safety.
Force measurement has a limitless number of applications to improve performance, maximize efficiency and even work in real-time to provide smart decisions. At Interface, we are discovering new ways to redevelop our load cell, torque and multi-axis sensor products for customized solutions to meet the growing demands for innovation.
Interface works with a wide range of industries, including aerospace, automotive, medical, metrology and industrial automation by teaming up to create unique use cases and applications that require our custom force measurement solutions. If you have a unique project that requires a custom solution, please visit the custom solutions page on our site at /custom-solutions/ or contact us at 480-948-5555.
Contributor: Ken Bishop, Sales and Custom Solutions Director at Interface
Tank-Weighing-and-Center-of-Gravity-1