Force Measurement Solutions Demonstrations at Automotive Testing Expo
Automotive Testing Expo. The focus of this year includes our multi-axis sensors, axial torsion and torque transducers, miniature load cells, wireless and testing rig solutions, instrumentation, along with our precision load cell technologies for all types of automotive testing and equipment used in the industry.
Interface experts are returning to Novi, Michigan, to demonstrate new and popular force measurement solutions at theNew SuperSC for Automotive Industry
One of the demonstrations will be Interface’s new SuperSC S-Type Miniature Load Cell. This new product is an economical general purpose load cell with a compact design that measures tension and compression in one unit. It offers high performance capacities in a form factor 80% smaller and 50% lighter than other models of s-type shear beam load cells.
The SuperSC is an ideal product in end of line validation testing for automotive, individual automotive component testing, and fatigue or life cycle testing. It is versatile for machines, component tests, integration into a manufacturing or assembly line for real-time force monitoring.
Many automotive testing labs rely on an actuator for fatigue or lifetime expectancy testing. Without force measurement, testers can only tell when the product reaches failure. The SuperSC can provide early warnings on component performance and life degradation.
SuperSC comes in 12 capacities ranging from 25 to 1K lbf and 100 N to 5 kN. Six designs for international standards of measurement (metric) and six for imperial standards. They are environmentally sealed with an IP66 rating and offer high stiffness with low detection and is insensitive to off-axis loading.
AxialTQ Demonstration
Another product that will be a focus is the revolutionary AxialTQ™ Wireless Rotary Torque Transducer. Designed for the automotive industry, this transducer is common for advanced torque tests and in the electric vehicle markets. Interface presented a new white paper that provides comparative research related to the AxialTQ product, demonstrating its performance related to other offerings. Read AxialTQ Technical White Paper Details Comparative Testing.
To learn more about AxialTQ, watch this video demonstration.
Automotive Testing Applications
Interface will also be showcasing brake pedal load cells, our robot using multi-axis sensors, digital and portable instrumentation and custom solutions designed specifically for auto test engineers. One of these solutions that we will be sharing is our Electric Vehicle Structural Battery Testing application.
EV Battery Structural Testing
Structural EV battery testing is core to optimization as innovation drives electric vehicle battery design and sustainability. Automotive manufacturers and component testing engineers need to validate structural battery pack design for life expectancy against design targets, as well as crash test compliance and survivability. Working with the EV battery maker, Interface’s recommendation is our 1100 Ultra-Precision LowProfile Load Cells for use in-line with hydraulic or electromechanical actuators within the test stand. Interface’s 6A Series 6-Axis Load Cells are also used to capture reactive forces transmitting through pack structure. Multi-axis measurement brings greater system level insight and improved product success.
Bluetooth® Brake Pedal Animated Application Note
Additional Automotive Solutions and Resources
EV Battery Testing Solutions Utilize Interface Mini Load Cells
Electric Vehicle Battery Monitoring App Note
Torque Measurement for Electric Vehicles
Automotive Head Rest Testing App Note
Fine-Tuning Testing Solutions for Championship Racing Vehicles
Automotive Window Pinch Force Testing
Automotive Head Rest Testing Animated Application Note