Hazardous Environment Solutions from Interface
There are hundreds of thousands of engineers and manufacturers that spend their days working in hazardous environments. Whether its operating inside of facilities with large machines with intricate moving parts, working hundreds of feet in the air repairing a bridge, or deep within a mine shaft, these professionals put themselves in danger every day by the nature of their work. As engineers and manufacturers, many of us are also tasked to solve for safety challenges and keep these professionals protected in any environment.
At Interface, one of the ways we contribute to industrial safety is with the development of our Interface Ex Rated Load Cells, also known as Interface Intrinsically Safe Products. These specialized load cells and force measurement solutions are designed and manufactured so that the materials and electronic components are safe for use in hazardous gas and dust environments when installed per applicable installation instructions. These components play an integral role in the safety of the men and women working in dangerous environments in particular industries like oil and gas, mining, aerospace, automotive and more.
These hazardous environments are categorized by the amount of explosive risk that is present in the environment. These levels include:
- Zone Zero – explosive presence is always there
- Zone One – explosive presence is close and is sometimes there
- Zone Two – explosive presence is nearby, but is rarely present other than in some type of leak or other catastrophes
In order for force measurement products to operate safely in these environments, companies must design the devices in accordance with a regulatory body. These products must also be inspected for approval and then it is marked with the certification code that displays the zone and temperatures it’s safe to operate in. In addition, the manufacturing process needs to be highly controlled. Manufacturers must keep documentation for each product, which includes how the product was made and where it went. And they are required to keep that documentation for 10 years in case of a product recall.
There are a number of different regulatory bodies focused on product safety throughout the world, and each has different specifications for explosiveness that need to be met based on the area in which the product is sold. Locations in which Interface can sell its Ex Rated products include countries in North America, Europe, Asia, and Brazil in South America.
The regulatory bodies that develop the specifications and approve products include:
- International Electrotechnical Commission Explosive Atmospheres (IECEx) is given after a manufacturer proves compliance through a quality assessment report (QAR).
- ATmospheres EXplosible or ATEX is a European Union(EU) examination certification. In order to receive ATEX certification, the manufacturer must obtain a quality assurance notification (QAN) to sell products in certain EU areas.
Interface develops a host of Ex Rated force measurement products that are certified by both IECEx and ATEX. These products have been used in a wide variety of applications within the energy and automotive industries. Included below are a few examples of the products we sell and the applications using our Ex products
ATEX 3400 Series Load Cells
The 3400 series of load cells are rated for Zone 1 and include the 3416 and 3430 Coil Tubing Intrinsically Safe Load Cells, the 3420 Coil Tubing Intrinsically Safe Load Cell and the 3410 Intrinsically Safe LowProfile® Load Cell. These products are hermetically sealed and have been used in the oil and gas industry to measure the force of coil tubing as it goes down an oil well. The 3400 Series is used in the space industry to help develop hydrogen-powered vehicles because of the threat of explosion with hydrogen power. The 3400 Series Load Cells have also been used in a distillery for a custom whiskey-making application.
ATEX, IECEx, ETL, Inmetro 1923 Series
The 1923 Series Load Cell is used in the oil and gas industry. These load cells include designs rated for both Zone 0 and Zone 2 applications. This load cell measures the force in which the pump jack is operating to avoid allowing the pump to go too fast and interrupt the capillary flow of oil. We also recently developed and released the 1923 Wireless Series load cell. Our 1923 Wireless Series innovation provides the same accurate, real-time data readings with little to no fuss over wires, which can create more hazards for the user.
ATEX SSMH Sealed Hazardous Environment Intrinsically Safe S-Type Load Cell
Our Zone 1 rated SSMH S-Type Load Cell is our only load cell that is certified for dust, so it is most often used in mining operations. This product is a tension and compression load cell that is environmentally sealed at an IP65 rating. It also has a high-temperature rating of up to 290° F for dust environments.
ATEX IECEx Bow Type Crosby™ Cabled Load Shackle
The Interface range of ATEX IECEx load shackles is designed for lifting and weighing in rugged or harsh environments, and also meet the requirements for operation in Zone 1 and 2 hazardous areas. The shackle pins are forged from high tensile stainless steel and are machined to an exacting specification. This range of load shackles is proof loaded to 150% of the normal rated load and is available in a range from 3.25 to 400 MT (7.17K to 882K lbf). The product is internally gaged and the whole instrumented area is sealed to IP67 to protect it in service.
When operating in explosive environments, our customers need to know that their products are safe and reliable. Here at Interface, we stand by the quality of our work and the safety of our Ex Rated products. For more information on Interface’s Intrinsically Safe and Ex Rated products, please visit /product-category/intrinsically-safe/.
Contributor: Ken Vining, Chief Engineer at Interface