How Load Cells Are Transforming the Construction Industry

The construction industry is one the most universal, growing, and dangerous industries in the world. Interface force measurement solutions are used for all types of construction applications from bridge and high-rise building projects to foundation load tests and structural monitoring. Our sensors and instrumentation are used in crane and heavy lifting operations, material testing and equipment calibration.

Accuracy and quality of all measurement products used for design, testing, monitoring, and equipment evaluations is imperative in protecting the project’s assets and workers. One of the leading causes of construction accidents is overloading equipment. When equipment is overloaded, it can fail, leading to serious injuries. It is essential to utilize high accuracy load cell technologies to measure the amount of force being applied to construction equipment.

Interface force measurement solutions can help to prevent overloading accidents by using the measurement data to ensure that equipment is not being extended beyond its safety capabilities. Force measurement solutions can also be used to monitor the performance of equipment and identify potential problems before they lead to an accident.

Interface offers a wide variety of sensor solutions for construction equipment and material testing. Our load cells offer precise measurements of applied forces, furnishing essential data regarding the structural response under various load circumstances. This data plays a critical role in evaluating structural integrity, detecting potential vulnerabilities, and optimizing design to guarantee the safety and dependability of infrastructure.

Interface force measurement solutions can help to improve efficiency and productivity in the construction industry in all areas including engineering, testing and maintenance. By monitoring the performance of equipment, construction companies can identify areas where they can improve efficiency.

It is common to find Interface load cells, including load pins, load shackles, miniature and even jumbo load cells in use for various forms of construction projects, equipment and tools. These products, as well as torque transducers, instrumentation and wireless systems are frequently used in the testing and monitoring of the machinery, rigging and lifting devices, gear, and heavy duty vehicles that are used in various stages of building.

Interface provides various sensors for a range of construction use cases around the world, including:

  • Residential and commercial buildings
  • Infrastructure programs
  • Industrial construction
  • Material testing machines
  • Civil engineering projects
  • Mining and tunneling
  • Environmental remediation
  • Heavy equipment manufacturing
  • Vehicle OEMS
  • Cranes and lifting equipment


Construction is an ever-present and ever-growing industry estimated to reach nearly $13T in global spending with broad and diverse use of measurement solutions. From single dwelling construction tools to heavy machines used to move concrete slabs, measurement is fundamental in construction. Included below we have provided a few examples of how our sensors are being used in construction.

Construction Reach Stacker

A reach stacker is a vehicle used in construction site to lift, move, and stack heavy containers. A force monitoring system was needed to ensure the safety of surrounding personnel, and if the reach stacker can lift heavy loads. Interface’s WTSLP Wireless Stainless Steel Load Pins were installed into the corners of the lifting mechanism of the reach stacker, where heavy loaded containers are lifted and moved. The force results were then wirelessly transmitted to both the WTS-BS-1-HS Wireless Handheld Display for Single Transmitters, or directly to the customer’s PC with the WTS-BS-6 Wireless Telemetry Dongle Base Station. Using this solution, the customer was able to monitor their reach stacker with Interface’s Wireless Telemetry System and ensure its ability to lift heavy loads on site.

Bridge Construction Wind Monitoring

Wind monitoring is a necessary operation during bridge constructions. Strong winds can destroy a bridge under construction since it is a work in progress with poor structural design. Monitoring these winds in real time is much more accurate than using predicted weather forecasts. Interface suggested installing the WTS-WSS Wireless Wind Speed Transmitter Module on the highest point of construction, such as a crane. Wind speed results were wirelessly transmitted to the customer’s PC through WTS-BS-4 Wireless Base Station with USB Interface in Industrial Enclosure. It was transmitted to the WTS-BS-1 Wireless Handheld Display for Unlimited Transmitters Data can be displayed, logged, and graphed with supplied Log100 software. Interface’s WTS-WSS Wireless Wind Speed Transmitter Module combined with Interface’s Wireless Telemetry System was perfect to monitor the wind speed in real-time during the bridge’s construction.

Metal Bending Force Material Testing for Construction

A construction material supplier wanted to know how much force it takes to bend different grades of steel metal used for building and infrastructure projects. They use their metal bending machine to create different metal hardware and wanted to record the amounts of force it takes to bend the metal used for their projects. Interface suggested using a wireless method, so cables do not interfere with the machine. The WTS 1200 Standard Precision LowProfile® Wireless Load Cell was attached to the head of the hydraulic operated steel bender. Results were wirelessly transmit to the customers PC through the WTS-BS-4 Wireless Base Station with USB Interface, where data can be displayed, logged, and graphed with supplied Log100 software. Using this solution, the customer was able to record the force results of his metal bending machine with Interface’s Wireless Telemetry System.

Interface is adept at providing solutions suited for use in construction projects, equipment and ongoing monitoring programs.  If you have questions about what products are suited for your specific project, equipment or testing programs, contact us. We are here to help.

ADDITIONAL RESOURCES

Force Measurement Solutions for the Construction Industry

Interface Solutions for Heavy Equipment

Gantry Crane Weighing

Lifting Heavy Objects

Rigging Engineers Choose Interface Measurement Solutions

Innovative Interface Lifting Solutions

Modernizing Infrastructure with Interface Sensor Technologies

Interface Solutions for Structural Testing

Why Civil Engineers Prefer Interface Products

Innovative Interface Load Pin Applications