Industry Leader in Test and Measurement
Interface was founded as a supplier of cutting-edge test and measurement industry solutions in 1968. It’s in our DNA and fundamental to what we’ve been engineering, manufacturing and selling for more than five decades. What started out as first to market with a pancake-style LowProfile load cell, has expanded into a broad mix of world-class test and measurement products and calibration services that enable T&M professionals full access to complete systems, from sensors to instrumentation.
Our mix of load cells, torque transducers, multi-axis sensors, calibration systems and other force measurement solutions allow engineers, product designers and manufacturers access to industry-leading testing devices that provide the most accurate and reliable data possible.
Whether that is testing the torque when applying a screw via robotics or verifying touch screen force for the latest 5G consumer hand-held device, we provide the sensors that test the machines, tools, and actual products before and in-market.
Interface is steadfast in ensuring the test and measurement professionals have more than quality sensors. We also provide T&M solutions to maintain and service testing equipment and devices used in labs and facilities throughout the world. The range of products we offer are from standard precision use to calibration-grade. Whether we are supplying our 1800 Platinum Standard Load Cell or a Verification Load Frame, Interface supports all types of T&M pros. Or as we like to call them, ForceLeaders.
Test and measurement use cases are growing due to the demands for miniature load cells, more data for intelligence gathering and automation functionality. It is estimated that more than $27B is spent in the production of test and measurement equipment globally. And the market is growing due to professionals seeking advancements in equipment and sensor technologies for use in new products, maintaining equipment and sustaining usability with data and proven testing rigor.
Interface sensors are involved in a wide range of T&M applications across a multitude of industries, with increased visibility into new markets like IoT and smart data-drive technologies.
Trends in test and measurement that are fueling the greatest growth:
- Medical and healthcare devices using miniature and wireless sensor technologies
- Activation of sensors into real-time data monitors and feedback tools
- Networking and communications use with 5G and wireless sensor capabilities
- Robotics and industrial automation machines and equipment
- Safety and regulation equipment with performance sensors
- Consumer electronics durability and usability
- Environmental exposure and changing conditions, from submersible to extreme temperatures
Read more about the trends in test and measurement in 2022 Test and Measurement Industry Trends.
The reason Interface is the industry-leading provider is because T&M requires precision and reliability. Interface sensors are known for being the most accurate in the industry. From structural and material testing to static and fatigue testing, our products provide key data for manufacturers, engineers and testing professionals to ensure their products and services will hold up under designed loads and performance standards.
From our Ultra Low Capacity series measuring forces in mere grams to our LowProfile™ load cells with capacities up to 2 million lbf, our solutions can meet the needs for any test profile required when it comes to force. In regard to torque testing, Interface can supply torque transducers with ranges as low as 0.005 Nm and up to 340K Nm to meet the needs of your test. Our overload protected low capacity load cells and torque sensor provide the most accurate results in the industry. In fact, T&M experts measuring torsion effects, tension tests, mass and kinetic energy are utilizing our products. Watch the video below to see some popular Interface Test and Measurement Product Solutions.
Interface provides an overview of solutions for the T&M industry, detailing our capabilities and providing an overview of some of recent applications. Of course, there are hundreds of use cases every year that depend on Interface, so these are just a couple highlights we thought you would find interesting below. Download the T&M Industry brochure at https://bit.ly/37q3Bnx. E-Bike Torque Measurement
An E-Bike manufacturer needed to test the torque on their electronic bicycles. They needed a torque sensing system that measures how much force the bike rider is pedaling onto the pedals, because this determines how much electric power the bike’s motor generates. Interface suggested installing the Model T12 Square Drive Torque Transducer where the pedal assist sensor would normally be. The T12 Square Drive Torque Transducer’s results can be recorded, graphed, and logged using the SI-USB4 4 Channel USB Interface Module when connected to the customer’s PC. Using this solution, the E-Bike manufacturing company successfully tested the torque on their electronic bicycles with Interface’s products and instrumentation. Read the full E-Bike app note here.
Proving Theoretical Cutting Forces of Rotary Ultrasonic Machining
Rotary ultrasonic machining is a hybrid process that combines diamond grinding with ultrasonic machining to provide fast, high-quality drilling of many ceramic and glass applications. This new method has been theoretically proven using computer models. Rotary ultrasonic machining generates forces of a very small magnitude. To prove this theory, any load cell used for measurement must be sensitive, while at the same time retaining high structural stiffness within a compact, low-profile envelope. Interface’s 3A120 3-Axis load cell is installed in the rotary ultrasonic machine to measure the forces being applied to a sample part. With clear signals and minimal crosstalk, the applied forces are recorded and stored using an the BSC4D Multi-Channel PC Interface Module. The 3-Axis load cell provides excellent data helping uncover the relationship between machine cutting parameters and the forces applied on the component. Using this knowledge, the machining process can be reliably optimized for new materials and operations. Learn more about this machining T&M app note here.
You can learn more about all types of T&M applications in our Applications Catalog, demonstrating the diversity and range of T&M solutions and ingenuity of our customers.
Request a Quote from Interface, The World Leader in Force Measurement Solutions
Additional Resources:
Interface Solutions for Testing Tools
Insights in Torque Testing Featured in Quality Magazine