Get an Inside Look at Interface’s Famously Blue Load Cells
Interface “blue” load cells have been utilized for millions of test and measurement projects and programs around the world. Since the invention of Interface’s LowProfile® Load Cell, the world’s most popular pancake style load cell series has become a standard for testing engineers and lab technicians for more than five and half decades. Today, Interface has more than 60 different types of Load Cells, including our line of Mini Load Cells.
Interface load cells come in capacities ranging from 1 lbf (500 gf) to 2 million lbf (9,000 kN). As a U.S.-based manufacturer, our extensive production and engineering facilities produce several shapes and sizes of our Interface load cells, as well as calibrate every model before it leaves our facilities.
Our expansive line of sensor models includes pancake and donut styled load cells in our LowProfile® Load Cell series and thru-hole load cells. Additionally, we offer canister, rod end, downhole, column, coil tubing, load buttons, and load washers. All of these models use Interface’s proprietary alloy strain gages to provide higher output, higher signal to noise ratio, higher resolution and superior fatigue life. This helps us build the most accurate and reliable sensors for test and measurement applications.
What makes Interface’s LowProfile Load Cells a top pick?
Here is a look inside our famous blue load cell, highlighting the top reasons Interface is selected for accuracy, quality and performance.
Interface’s load cell model that has the highest demand and usage is the 1200 Precision LowProfile series. They are used in all types of industry applications, from Material Tensile Testing to Aircraft Lifting Equipment Tests. It’s followed closely by the 1000 Fatigue-Rated LowProfile series and 1100 Ultra Precision Load Cell series. Every series has multiple configuration and capacity options. For example, the 1200 series provides off-the-shelf model options including:
1200 Standard Precision LowProfile® Load Cell
1200 and 1201 Series 3-Wire Amplified Load Cell Universal or Compression-Only
WTS 1200 Standard Precision LowProfile® Wireless Load Cell
1200 High-Capacity Standard Precision LowProfile® Load Cell
1201 Compression-Only Standard Precision LowProfile® Load Cell
Every designed load cell can also be engineered-to-order or customized to unique specifications.
The accuracy of data, engineered designs, proprietary strain gages, comprehensive specifications, quality inspections, detailed certifications and multiple calibrations of every load cell to ensure performance make the top of the list as to why Interface is considered best in class.
Here is an opportunity to get another inside look at the Interface LowProfile Load Cell:
If you are interested in reviewing this insider’s view with SI measurements, go here.
Take a closer look at the advantages of Interface’s LowProfile Load Cell in this cutaway view.
LowProfile Cutaway