Interface Load Cells Propel New Torsional Force Measurements for Wind Energy Project
Amongst the wide variety of industries that Interface serves, clean and renewable energy sectors are some of the hottest in pursuit of sensor-based solutions. Between private and public funding, and the overwhelming desire for humans to become more sustainable, new energy technology and investment is multiplying at a rapid pace.
Interface force measurement solutions are used in all types of energy-related applications for wind, solar, hydro, nuclear, geothermal, and emerging energy sources worldwide. We are recognized as a provider of choice for our reliability and accuracy in designing, engineering, testing, innovating, and manufacturing precision sensor solutions for the energy industry. In fact, we have designed unique load cells that are embedded into some of the largest test and production equipment for energy production in the world. Read Interface Most Promising Energy Tech Solution Provider
Advance technologies in renewable and sustainable energy sources continues to drive the critical need to monitor, test, and validate concepts, equipment, and tools used in procurement. In the global energy industry, many of the alternative source technologies are inventive, newer, and require unique measurement solutions to take on the challenges found in R&D, testing, and production.
In addition, alternative energy sources in their infancy can be very cost prohibitive going from exploration to consumption. Therefore, it is important that quality, cost effective testing solutions are provided to help researchers, engineers and manufacturers minimize total costs. Interface force testing solutions help to solve and lessen the burden of these challenges by offering a wide range of test and measurement solutions.
New Interface case study reveals how our load cells were used by the PTB in Germany to calibrate and test the world’s largest machine that measures torsional forces related to wind turbines.
Interface force measurement sensors were requested to help Physikalisch-Technische Bundesanstalt (PTB), the national metrology institute of the Federal Republic of Germany, in the design of an innovative wind energy project. As the second largest metrology institute in the world, the PTB has an acclaimed international reputation in research relating to units and precise measurement.
PTB is a service provider for science, business, and society, and advises the German federal government on all metrology issues. Organizationally, the PTB is a departmental research facility and senior authority within the portfolio of the Federal Ministry of Economics and Climate Protection. For more than 135 years, PTB’s role has been making important contributions to advancing the energy transition, heat transition and climate protection with quality and speed.
Interface, working in tandem with our esteemed partner Interfaceforce e. K. in Germany, was asked to provide load cell solutions to use in the design and testing of the world’s first traceable torque measurements of up to 5 MN ∙ m for a wind energy facility. As a first of its kind project, the PTB needed to include high accuracy, quality test equipment to guarantee precise and reliable data. Interface solutions fit the exact requirements. Read the complete case study here.
Summarizing the engagement, PTB endeavored to construct a system with highly accurate and repeatable results, and one that enable bending moments, axial forces, and dynamic excitations of up to 3 Hz. Thereby, making it possible to realize a metrological characterization of dynamic influences in the (MN ∙ m) torque range, as well as in the MN force range. Working closely with PTB, Interface’s experts in Germany worked with the metrology lab engineers to identify the correct products for this unique calibration system.
These products are being used to calibrate and test PTB’s torque measurement system, allowing the system to provide accurate and repeatable results over time. The custom load cell products Interface provided PTB for this innovative wind energy system, as detailed in Interface Supports Incredible Wind Energy Innovation, included:
- Series 1208 Model 1258 Flange Precision LowProfile® Load Cell with 2nd bridge and two moment bridges for My and My
- Series 1208 Model 1248 Flange Precision LowProfile® Load Cell with 2nd bridge and two moment bridges for My and My
- Series 1200 Model 1220 Universal Precision LowProfile® Load Cell
- Model SM Super Mini High Accuracy S-Type Load Cell
The load cells that were chosen helped PTB to create the system needed for its wind energy facility, which allows multi-component transducers to be calibrated in a traceable and practice-oriented way for force and torque. The system is also now the world’s largest machine starting up at PTB, with which the large torsional forces that occur in wind turbines can be precisely measured for the first time. Read the article: World’s largest device for measuring torque in wind turbines opens.
As we detailed in Load Cells for Renewable Energy Production and Testing, Interface and our incredible distributor network continues to work with engineers and industry leaders to find viable measurement solutions. Pushing the boundary forward on new and renewable energy is rewarding for our company, especially as we help those achieve energy innovation using sustainable, quality measurement solutions.
Request a Quote from Interface, The World Leader in Force Measurement Solutions
ADDITIONAL RESOURCES
Interface and Green Energy Innovation
Interface Solutions for Growing Green Energy
Demands for Quality Energy Measurement Solutions
Interface Supports Renewable Energy Innovation
Interface Supports Incredible Wind Energy Innovation