Interface Solutions for Consumer Products
Interface’s force measurement solutions affect every industry and all types of products. Chances are that the everyday consumer has purchased and used something evaluated with or utilizing an embedded force sensor.
In fact, Interface has a long history in providing load cells and sensor technologies to test and measure consumer packaged goods (CPG) and products. They are commonplace in early-stage prototype testing, all through final distribution. Most often, our force measurement solutions help predict failure and identify design challenges before goods are available to consumers. It is hard to imagine any product that would not go through rigorous test and measurement protocols before it goes to market. The liabilities are too great and consumer safety is paramount.
It is also critical to use accurate, quality sensors to gather reliable user data related to any consumer product. Product makers use sensor data to assess product usability, capabilities, and durability. The more data, the greater the opportunity to adjust and ensure the product is a direct fit. Precision in this process through data will improve the product’s performance and influence adoption.
From testing home health care devices to ensuring household appliances are safe and durable, Interface’s sensor measurement technologies have a vital role in R&D, design, production and packaging. Load cells and other sensor products are used for all kinds of testing, from material to fatigue, in the creation and manufacturing of everyday goods. They are growing in popularity to make products smarter and designed for IoT use.
Consumer Product Applications for Interface Force Measurement Solutions
- Smart home devices
- IoT solutions
- Production line testing
- Usability research
- Safety and compliance
- Regulatory and performance monitoring
- Manufacturing robotics
- Warehouse equipment
- Food packaging
- Toys
- Gaming and simulation equipment
- Electronics hardware
- Sports equipment
- Furniture
- Capping and bottling machines
- Real-time user feedback
We even provide products to accurately measure and monitor hardware used in intermediate goods, assembly equipment, and distribution. Our force measurement solutions are ideal for consumer product stand-alone testing rigs, production equipment, as well as embedded in consumer products to increase operability and reliability for end users.
Interface load cells and instrumentation help product designers and fabricators drive usability, adoption, production efficiencies, and ensure safety to satisfy the needs of all types of consumers. Here are a few applications notes to demonstrate Interface solutions utilized in the consumer products industry. Additional applications for consumer packaged goods and consumer products are found here.
Commercial Food Processing
A consumer food product processing plant wants to measure in-motion the food weigh as it is processed down the line. They want to ensure production line efficiency and food quality for future consumers. The customer also wants real-time results of their food being weighed to keep standards high and ensure quality product. Multiple of Interface’s SPI High Capacity Platform Scale Load Cells can be installed in the customer’s in-motion check weigher at the specific points where the food is weighed on the belt to deliver precise weighing results. When connected to the 920i Programmable Weight Indicator and Controller, real time results of the weight of the food being processed is available at all times. The 920i Programmable Weight Indicator and Controller can read up to four scale channels. Read more here.
Computer Touchpad Force Testing
A laptop manufacturer wanted to test their mouse touchpads to ensure it is functioning properly for future consumers, thus measuring the right amount of sensitivity during the consumer’s use. They also needed a system that measures the force it takes for the mouse pad to activate a response on the laptop. Interface suggested using the SMTM Micro S-Type Load Cell, from the Interface Mini™ line. The SMTM was installed in the customer’s actuator test rig. The SMTM recorded the amount of force it takes to press on the trackpad and create a response on different areas of the trackpad. An actuator aided with tactile feedback by providing movements such as dragging or creating friction. The measurements were captured using the 9330 Battery Powered High Speed Data Logging Indicator through an SD card, or another laptop directly. The SMTM Micro S-Type Load Cell was able to measure the forces applied to the mouse touchpad at various locations. Interface’s products successfully measured the forces needed to make the mouse touchpad create a response. Get more information here.
Furniture Fatigue Cycle Testing
To meet safety protocols in relation to the manufacturing of various furniture products, rigorous fatigue testing, shock testing, and proof testing before dispersion into the marketplace, and into the homes of consumers. Force testing on furniture products is critical in determining the posted max loads to protect manufacturers from liability due to damages that might result from the misuse of those products and overloading. Using Interface’s SSMF Fatigue Rated S-Type Load Cell along with Interface’s 9890 Strain Gage, Load Cell, & mV/V Indicator provides a solution that measures the force being applied in fatigue cycle testing of a furniture product, in this case testing the rocking mechanism in an office chair. Unlike other similar load cells, the SSMF is fatigue rated making it highly suitable for fatigue testing. Using this solution, the furniture manufacturer was able to obtain accurate data about the rocking mechanism the office chair as it was fatigue cycled into failure. Post testing, adjustments to the design to improve the safety and life of the furniture, ensuring product quality, and protecting the manufacturer from future liability. Learn more here.
Printer Cartridge Seal
An ink manufacturer wanted to ensure there is a proper seal between their ink cartridge caps and the cartridge body, for it to work effectively in their printers and for consumers buying it for themselves. A bad seal can cause leaks, clogging, and overall deficient performance for their printers. Interface’s solution was to measure the pressure exerted on the cartridge cap by installing the 3A120 3-Axis Load Cell under the plate during the automatic production line process. Results were logged, graphed, and stored when the customer’s PC or laptop is connected to the BSC4D Multi-Channel PC Interface Module with supplied BlueDAQ software. Using this solution, the ink manufacturer was able to determine the exact amount of force it took to seal their ink cartridge caps onto the cartridge bodies to prevent any leaks or clogging. Learn more here.
Interface solutions for consumer products are abundant. For every machine, test system and even many products themselves, these products benefit from a force sensor to improve product performance, prove reliability and more.
Additional Resources
Force Measurement is Reducing Waste and Automating the Consumer Packaging Industry
Applications for Consumer Products and Packaging
Load Cells for Consumer Product Applications
CPG Bike Handlebar Fatigue Testing
Interface Solutions in the World of Sports
CPG Water Bottle Dispensing and Weighing