Interface Solutions for Industrial Markets

The industrial market is vast. The industry classification covers everything from manufacturing and assembly to mining and agriculture. The highly regulated environments involved in industrial applications often require advanced equipment and technologies for product design and development, as well as after market performance management. Force and torque products are critical sensor components used in industrial applications.

Interface has been a partner to industrial customers for more than 50 years. We engineer, build, and supply force and torque sensors and acquisition devices designed to provide industrial engineers and manufacturers with high quality data that monitors and confirms the design and in-action processes of their equipment. Applications for industrial markets involve everything from heavy machinery to weighing solutions. The accuracy of these devices is critical to high-quality outcomes, low-costs and most importantly, worker safety.

INDUSTRIAL APPLICATIONS 

An example of an industrial process that requires an accurate force sensor is a crane application used in lifting heaving objects. Interface engaged with a customer who needed to measure the lifting capabilities of a crane using an Interface load shackle. The purpose of the shackle was to ensure the crane wasn’t lifting more than it could handle, putting worker safety at risk and potentially damaging the machine.

Interface model WTSSHK-B Wireless Load Shackle was connected to a crane load string to measure forces. A model WTS-BS-1-HA Battery Powered Handheld Display was used to wirelessly receive load information and display results. Using this solution, the customer was able to successfully measure lifting and reading weight wirelessly on a handheld display while the crane was in action.

Another great example of the industrial industry’s use of force applications can be seen in manufacturing automation. One of the growing trends in marketing automation is the use of robotics to replace repetitive human tasks. Robotic arms are often found on assembly lines and they carry out a single task over and over. If the robotic arm isn’t properly calibrated, it can ruin an entire production line and lead to significant losses. To qualify the accuracy, many OEM’s use load cells and torque transducers to continuously measure the intricate movements of a robotic arm.

One Interface customer used a robotic arm to close packaging on a production line. If the arm wasn’t accurate, it could apply to much force and crush the packaging or not close the packaging as intended, leading to losses in shipping.

Interface supplied a 6-Axis Load Cell with a model BX8 Data Acquisition and Amplifier System. The Interface Multi-Axis 6-Axis Load Cell was able to measure all forces and torques on every axis and the BX8 8-Channel Data Acquisition System was able to log, display, and graph these measurements while sending scaled analog output signals for these axes to the robot’s control system.

READ MORE HERE: FORCE MEASUREMENT IS REDUCING WASTE AND AUTOMATING THE CONSUMER PACKAGING INDUSTRY

Another consideration for specialized industrial applications is in harsh environments. There are hundreds of thousands of engineers and manufacturers that spend their days working in these environments. Whether its operating inside of facilities with large machines and intricate moving parts, working hundreds of feet in the air repairing a bridge, or deep within a mine shaft, these professionals put themselves in danger every day by the nature of their work. As engineers and manufacturers, many of us are also tasked to solve for safety challenges and keep these professionals protected in any environment.

One of the ways we contribute to industrial safety is with the development of our Interface Ex Rated Load Cells, also known as Interface Intrinsically Safe Products. These specialized load cells and force measurement solutions are designed and manufactured so that the materials and electronic components are safe for use in hazardous gas and dust environments when installed per applicable installation instructions. These components are designed for those applications found in dangerous environments in particular industries like oil and gas, mining, aerospace, automotive and more.

The applications for industrial vary widely because the industry is diverse. Interfaces designs and manufacturers force and torque products for hundreds of different industrial use cases and applications every year. Our team of engineers can even create custom solutions for new and innovative industrial requirements. Included below are examples of some of the products typically used by our industrial customers.

  • 2400 Load Cell Series – The 2400 is a stainless-steel load cell designed for applications requiring a hermetic seal for use in general industrial applications.
  • 3200 Load Cell Series – The 3200 precision stainless steel load cell series has all the features of the Interface Model 1200 LowProfile® (one of Interface’s most popular products) and in addition it is stainless steel and hermetically sealed for harsh applications.
  • SSMH Load Cell Series – Model SSMH S-type load cell provides a suitable force measurement sensor for applications in coal mining and transfer and other heavy industries where explosive dusts and environment conditions are potentially explosion-hazard rated. SSMH capacities available that provide intrinsically safe certification.
  • Stainless Steel Load Buttons – Interface’s load button load cells are designed for customers who require the measurement of forces in a very confined space. They are designed to provide the most accuracy in as little space as possible.
  • 5400 Series Reaction Torque Transducer Series – Model 5400 series features a rugged flange-style designed with thru-holes, low deflection, high torsional stiffness and the ability to withstand large overhung moments.
  • Wireless Telemetry System (WTS) – High accuracy, high quality measurement is interfaced with simple yet powerful configuration and monitoring software. The WTS gives sensor manufacturers and integrators the complete flexibility to build their own sensor modules around it. The system easily replaces wired systems, reducing installation and maintenance costs.

These are just a few examples of Interface applications notes and products designed for industrial applications. For more information on Interface solutions design for the Industrial industry, contact our experienced application engineers.