Interface Solutions for Lifting Applications
Often large capacity load cells are used in industrial equipment, cranes, forklifts, rigging, and even aircraft testing equipment to measure forces applied in heavy lifting and for load monitoring, as well as to maintain accuracy in movement. Larger capacity load cells can range from 10,000 to million lbf, or even larger. Rugged load cells are frequently selected for this type of equipment to sustain harsh environmental conditions for both testing and during real-time use.
Smaller capacity load cells, such as s-types and miniature beams, measure the lift action in machines, medical equipment, packaging, robotics, drones and moving equipment. In all circumstances, force measurement sensors help product engineers and manufacturers improve safety and the quality of products they build. They are versatile and easily integrated into machines and components.
Beyond the measurement specifications, other top feature considerations when selecting the right sensor include weight of the sensor, requirements for overload protection, enclosures and ruggedized material used to construct the device, signal outputs for data, cabling, or wireless functionality, mounting or clamping, and instrumentation for data acquisition.
For measurement in lifting applications, Interface products provide the industry’s most accurate and reliable data available through force measurement sensors. Products we provide for lifting include multi-axis sensors, load washer load cells, low profiles, miniature load cells, load shackles, load pins, tensions links, instrumentation, and torque transducers.
The following are examples of products we supply for lifting equipment and use cases.
AERIAL BOOM LIFT OPERATION
3AXX 3-Axis Force Load Cell model 3A160 to capture the required data for monitoring in real-time. Paired with the 920i Programmable Weight Indicator and Controller, the operator had accurate information when using the equipment.
A manufacturer aerial lifts wants to test its self-propelled boom platform to ensure it can operate at heavy capacities when in use, and at different angles. This testing is vital for safety and protecting operators as well as those at the site of where equipment is in use. The sensors help to prevent any accidents in case of a lifting overload. The Interface application engineers recommends the multi-axisAIRCRAFT LIFTING TEST RIG
An aerospace manufacturer is looking to accurately measure the valves in their aircraft lifting test equipment. Interface’s solution is to install a 1200 High Capacity Standard Precision LowProfile™ Load Cell in between the aircraft testing rig and the lifting jack. The load cell will measure the load’s force safety valve when the lifting equipment opens. Results will be sent to the 9890 Strain Gage, Load Cell, & mV/V Indicator, where the customer can see it displayed in real-time.
LIFTING HEAVY OBJECTS
WTSSHK-B Wireless Load Shackle connected in crane load string to measure forces. Model WTS-BS-1-HA Battery Powered Handheld Display is used to wirelessly receive load information and display results.
In this common use case, a customer needs to measure the load when using a crane to move heavy construction materials around the work site. This includes monitoring the weight of these objects as they are lifted in the air. It was critical that the device offer high accuracy readings and also work within the equipment already in place. Key is the instrumentation capabilities to provide wireless outputs. Interface recommends using ourRead more about these types of lifting applications in our new case study. If you need help in deciding which product works best for your lifting application, contact us.