Interface Solutions for Machine Builders
No matter the industry, if products are being made chances are industrial machines are involved in some part of R&D, testing, production, and distribution.
Engineers involved in the design and manufacturing of these machines require the highest quality sensors, tools and equipment. In addition, humans often lean on machines for very precise or repetitive tasks, this means that precision and reliability is key for every aspect of these machines.
Machine builders are the backbone of product development and production. They are responsible for building, assembling, and integrating components for stand-alone and multi-station automated machine tools and systems. These automated machine-tool systems are used in all sectors of manufacturing, including assembly, processing, and fabricating systems.
Interface plays a critical role for machine builders, for those that design one machine or manufacture machines at scale for users around the world. We supply machine builders with precision load cells, torque transducers, instrumentation, data acquisition devices and accessories. They lean on Interface because of our experience in supplying the world solutions utilized for industrial product testing and production across all kinds of industries from agricultural machinery to medical testing machines.
The accuracy and quality of our products is why machine builders rely on Interface. In addition, our experience and diversity of product has led machine builders and engineers to choose Interface force measurement sensors throughout their careers. In fact, Interface has served machine builders for more than 50 years. It is a relationship and role we know very well.
The world of machine building has also changed over the years. In the past, machine builders used force sensors primarily to test products before going out to the market. This is still a prominent use case amongst product engineers. The fast-rising use cases over the past decade comes from the demand for smarter machines, automation and miniaturization of products.
Today, more machines builders and OEMs are designing force sensors directly into machines to allow users to activate components, monitor data on the machines in use for real-time feedback and adjustments. This type of innovation using sensors has opened opportunities for Industry 4.0 connectivity between machines.
To get a better idea of how machine builders are using force sensors, Interface has developed a wide range of applications notes to provide real world examples of force measurement in action in the machine building world. We have included a few of those examples below.
A customer wanted to test the amount of force it takes to cut through different thicknesses of metal on their metal press cutting machine. They also wanted to ensure their metal press cutting machine is working properly and understand its maximum limitation. Interface suggested installing their 3AXX 3-Axis Force Load Cell underneath the plate where pieces of metal are placed to be cut, or punched holes in. When connected to the BX8-HD44 BlueDAQ Series Data Acquisition System, the force results of different metals being cut will be displayed, graphed, and recorded on the customer’s PC. It also has an analog output that can connect to the machines PLC in case of an overload. Using this solution, the customer was able to determine the different number of forces it took for their metal press cutting machine to cut through different types and thicknesses of metal. Read more here.
Snack Weighing and Packaging Machine
A snack manufacturing brand wanted to weigh the amount of their snacks that is automatically dispersed into the bags during the packaging process. In this case, they wanted to weigh their potato chips being packaged and ensure the potato chips are at the exact weight needed due to regulatory standards. Interface’s solution was to use multiple SPI Platform Scale Load Cells and install it to the potato multi-head weigher and packaging machine. The SPI Platform Scale Load cells were installed inside of the mount that attaches the head weigher to the packaging machine. Force results from the potato chips are read by the load cells and sent to the ISG Isolated DIN Rail Mount Signal Conditioner, where the customer is able to control the automated production from their command center. Using this solution, the customer was able to determine the weight of the potato chips being distributed into their bags with highly accurate results. They also were able to control the automated production process with the provided instrumentation. They will use this same weighing method for other snacks that need to be packaged. Read about this application here.
Tablet Forming Machine
A pharmaceutical company needs to precisely monitor the forces applied by the tablet (pill) forming machine to understand the relationship between raw material, die set, forming force, and motor cycle speed. Optimizing the equipment will improve productivity and efficiency of the tablet forming process, while reducing losses. For maximizing production and monitoring the process, Interface suggested a WMC Sealed Stainless Steel Mini Load Cell (10K lbf Capacity) be mounted in the section of the downward press bar. The load cell was then connected to a 9320 Portable Load Cell Indicator to collect the needed data. Read more here.
Machine builders require the best test and monitoring equipment. Interface has backed professional machine builders, machine design engineers, machine manufacturers and those that utilize the equipment for many years with top-of-the-line force sensing solutions. Whether you are looking to build a machine, design machine tools and equipment or embed sensors into machines, we are here to help.
ADDITIONAL RESOURCES
Proving Theoretical Cutting Forces of Rotary Ultrasonic Machinery App Note
Force Solutions for Testing Machines
Interface Sensors Used for Internet of Things
Fitness Equipment and Machines
GS-SYS04 Gold Standard® Portable E4 Machine Calibration System