Introducing Interface Load Cell Selection Guides

When it comes to breadth and depth of sensor solutions, Interface has more than 35,000 products and countless options for customization. This can make choosing a specific load cell, torque transducer or instrumentation device for your next test project seem like a daunting task.

Our goal is to make your selection process easier. In addition to our global network of partners and team of Interface applications engineers, our online Interface Guides are resources designed to help you find the right measurement solution based on your exact requirements.

Recently, we have released two new selection guides to assist you in choosing the best load cell products, the Interface Load Cell Selection Guide and Interface Mini™ Load Cell Selection Guide. The two new Interface load cell selection guides offer a simple drop down menu for filtering the characteristics and model options of our extensive line of load cells. In addition, we provide a checklist for specific features that are best suited for your application and the environment in which you are utilizing the devices for testing and monitoring.

If you are not sure of what you need, we also include a helpful guide below each selection guide to walk you through the distinct types of load cells and their capabilities. Each selection will provide references to existing standard products that meet your criteria with easy links to additional specifications.

INTERFACE LOAD CELL SELECTION GUIDE

The Load Cell Selection Guide begins with criteria that will help you to narrow your options, including load cell types, options, features, and capabilities. Once you have selected one or more of the types to explore, each option will provide you a quick view of the product, capacities, and a link to detailed specifications, drawings, and datasheets. Start by selecting the model that provides the best fit based on the following types:

  • 2-Axis
  • Amplified
  • Axial Torsion
  • Calibration Grade
  • Canister
  • Column Rod End
  • Compression Only
  • Eccentric Load Compensate
  • Fatigue-Rate
  • Flange Mount
  • Intrinsically Safe
  • Moment Compensated
  • Overload Protected
  • Sealed
  • Stainless Steel
  • Submersible
  • Tension and Compression
  • Wireless

With every guide, Interface provides several technical references that are helpful in learning the ins-and-outs our load cells. As part of the Load Cell Selection Guide, you can review the technical make-up of our load cells, details about our proprietary strain gages, calibration insights, plus critical high-accuracy and quality performance parameters that set our products apart from the competition. You can also learn about the effects of temperature, moment compensation, and options available to support a variety of applications.

INTERFACE MINI LOAD CELL SELECTION GUIDE

For the Mini™ Load Cell Selection Guide, we provide a list of our popular miniature load cells with a detailed explanation of each model group. These descriptions provide an overview of the various features and capabilities of our mini products to help you choose the best solution for your use case. The products included in the Mini Load Cell Selection Guide include:

  • Load Cell Load Buttons
  • Load Washers
  • Bending Beam Load Cells
  • Double Bending Beam Load Cells
  • Sheer Beam Load Cells
  • S-Beam Load Cells
  • Overload Protected S-Cells
  • Single Point Impact Load Cells

These guides provide you with a solid baseline of information for making the right selection for your next project or for designing a sensor into your machine, product, or component. If you need further help or require an engineered-to-order or custom product, reach out to our experts. We are here to help!

For an all-time great load cell 101 reference, listen in as our top engineers detail load cell basics in this Interface Classic Series recorded webinar.

Additional Resources

How Do Load Cells Work?

Interface Load Cell Field Guide

Torque Transducer Selection Guide

Contributing Factors To Load Cell Accuracy

LowProfile Load Cells 101

Webinar Recap of Taking Measure of Miniature Load Cells

Interface Presents Load Cell Basics