Measurement Technologies for Boats, Yachts and Watercraft
maritime industry. Learn how our products play a big role in a wide variety of test and measurement applications for waterborne vessels, maintenance and safety equipment. Our load cells and instrumentation are found in offshore products, as well as at docks and in the open water. We have captured some of these specific use cases of how our sensor technologies and instrumentation are used in the building and maintenance of boats, yachts, and watercraft of all sizes.
Interface has been a long-term supplier of force and torque measurement solutions for theOur load cells and sensors work well in vehicles that are used in water. For example, we offer technologies that can wirelessly transmit data underwater and in harsh weather conditions, making them perfect for a variety machines used in water. These specialized load cells operate in underwater submersions at different capacities, and reliably relay information to those at the surface level for accurate sensor readings. Interface load cells of various designs can regulate harsh maritime situations in use cases such as underwater tension lines, underwater oil drilling, as well as storm and tsunami monitoring. Read more about offshore and near shore solutions here.
The applications we are highlighting below provide real-world examples of force measurement products used in boat, yacht and watercraft related products. The uses of force measurement range from testing fishing wire to yacht rigging inspection. Here’s a closer look:
Wireless Telemetry System (WTS) for Yacht Rigging Inspection
For a customer who wants to have a complete yacht rigging inspection to make sure the mast, still lines, and all movable hoisting lines are functional, Interface offers our robust WTS product line. These various wireless sensor technologies and components are designed for use to meet the proper specifications for sailing, testing the tension of the forestay, shroud, and backstay cables, and to test the tension of the movable lines when sailing.
With Interface’s WTSSHK-B Wireless Crosby™ Bow Load Shackle paired with the WTS-BS-1 Wireless Handheld Display for Unlimited Transmitters, the customer can switch and view between multiple shackles being tested. The WTS-BS-4 USB Industrial Base Station can also be attached to the customer’s computer to display real-time measurements from the shackles and log data. With this solution, the user is able to conduct both running and standing rigging inspections of their ship or vessel, and determine if all lines were functional and met safety standards. Read the entire WTS solutions used on this yacht here.
Commercial Fishing Wire Rope Testing
When a commercial fishing owner wanted to measure the force tension of the wire fishing rope connected to the fishing cage or net when their vessel goes to catch and ensure the wire rope is strong enough and safe enough to hold the maximum capacity of fish caught in the cage or net, they can turn to Interface.
Using a WTSTL Wireless Tension Link Load Cell attached between the end of the cable, and the end that hooks onto the fishing net, the tension link will be able to measure the forces of the full net of fish, or a heavy load at maximum capacities. The data information can be transmitted to both the WTS-BS-1-HS Handheld Display for Single Transmitters, or to the customer’s computer using the WTS-BS-4 USB Industrial Base Station. Utilizing this solution, the customer was able to determine if the fishing cable on their vessel was strong enough to hold the fish cage or net at maximum capacity when out catching.
Mooring Line Tension Testing
Due to changing environmental conditions, mooring cable lines undergo wear and tear. A customer wanted to ensure all mooring lines for ships and large commercial vessels are securely docked at the same loading tension, so that they do not risk the mooring lines to break or cause damage.
We provided a WTSTL Lightweight Wireless Tension Link, which can be attached to each mooring cable in use. Results are sent to the customers through the WTS-BS-4 USB Industrial Base Station when connected to the customer’s supplied computer. Data can also be transmitted to the WTS-BS-1-HA Handheld Display for Multiple Transmitters, giving the customer the option to view multiple mooring cable line tensions. The customer was able to verify the tensions to multiple mooring cable lines. Thus, resulting in the security of their ship being safely docked.
If you’re interested in learning more about our maritime solutions, call 480-948-5555 to contact an application engineer about your project requirements.