Solution
Aircraft Lifting Equipment
An aerospace company wants to check if the valves on their aircraft lifting equipment is working safely and properly.
An aerospace company wants to check if the valves on their aircraft lifting equipment is working safely and properly.
Interface’s solution is to install a 1200 High Capacity Standard Precision LowProfile™ Load Cell in between the aircraft testing rig and the lifting jack. The load cell will measure the load’s force safety valve when the lifting equipment opens. Results will be sent to the 9890 Strain Gage, Load Cell, & mV/V Indicator, where the customer can see it displayed in real-time.
The customer was able to determine that the aircraft lifting equipment was working properly. Since they are ensured of its safe functionality, it can now be used on real aircrafts that need to be lifted.
Notifications