Solution
Feed Roller System
A customer has a feed roller system, and needs to monitor the forces of both ends of the rollers, in order to maintain a constant straight feed. They would also prefer a wireless system.
A customer has a feed roller system, and needs to monitor the forces of both ends of the rollers, in order to maintain a constant straight feed. They would also prefer a wireless system.
Interface suggests installing two PBLC Pillow Block Load Cells at both ends of the bottom roller to measure the forces being applied. The forces are measured when connected to WTS-AM-1E Wireless Strain Bridge Transmitter Module. The data is then transmitted wirelessly to the WTS-BS-6 Wireless Telemetry Dongle Base Station and the WTS-BS-1-HA Wireless Handheld Display for multiple transmitters, where data can be displayed, graphed, and logged on the customer’s PC or laptop.
The PBLC Pillow Block Load Cells installed at the bottom roller was able to measure and monitor the forces to maintain the straight feed by the rollers.
Notifications