Interface sensor technologies and solutions find extensive usage in the global construction sector for monitoring and controlling the loads encountered during the construction projects. From bridges and dams to high-rise buildings and tunnels, measurement devices and instrumentation are utilized by civil engineers, heavy equipment manufacturers, material engineers, and test labs to accurately measure and test weight, force, and torque across a variety of use cases.
The massive global construction industry, estimated to be nearly $13T in spending, is broad and diverse in use of measurement solutions. From single building tools to heavy machines used to move concrete slabs, measurement is fundamental in construction design and use for projects, tools and heavy equipment.
Interface products for test and measurement in this diverse industry are used in:
- Residential Construction
- Commercial Construction
- Infrastructure Construction
- Industrial Construction
- Civil Engineering Projects and Construction
- Mining and Tunneling
- Environmental Remediation
- Specialty Projects
- Heavy Equipment Manufacturing
- Transportation and Vehicle OEMs
- Cranes and Lifting Equipment
Interface load cells offer precise measurements of applied forces, furnishing essential data regarding the structural response under various load circumstances. This data plays a critical role in evaluating structural integrity, detecting potential vulnerabilities, and optimizing design to guarantee the safety and dependability of infrastructure.
Products we commonly supply to construction industry participants include:
- Load Cells
- Miniature Load Cells
- Torque Transducers
- Scales
- Multi-Axis Sensors
- Load Pins, Load Shackles and Tension Links
- Instrumentation
- Digital, Wireless and Bluetooth Solutions
- Custom Solutions
Load cells also are commonly used in construction equipment including cranes, hoists, and lifts. By incorporating Interface’s load cells into these machines, construction operators can reliably ascertain the loads being lifted or moved, ensuring compliance with secure operational thresholds.
By providing real-time load data, Interface’s load cells enable engineers and construction industry players to make informed decisions regarding the structural design, material selection, and load capacity of different machines and equipment. Torque transducers assist in evaluating and monitoring static and rotary movements of objects like motors and tools. Instrumentation is used to gather the data from measurements, which can influence design and be used as embedded technologies to give real-time feedback in use, just as in cranes and lifts.
Safety is of the utmost importance in the construction sector. Severe failures in equipment can be dangerous to machine operators, and protection and safety for users can be used through the use of force sensor technologies with Interface’s precision load cells, torque transducers, load pins, tension links and load shackles.
Applications of Force Measurement Products Used in the Construction Industry:
Bridge Construction: Load cells are employed in bridge construction to monitor the loads experienced by different components such as piers, beams, and cables. They help ensure that the bridge can handle the anticipated weight and forces and provide valuable data for load testing and structural analysis. Bridges also use sensors to provide ongoing monitoring of environmental changes, as noted in our case study Monitoring Seismic Force of a Suspension Bridge.
High-Rise Building Construction: For structural support, load cells are used during the construction of tall buildings to measure the loads exerted on structural elements like columns, slabs, and foundation systems. They assist in evaluating the structural integrity, optimizing design, and determining load distribution for safe and stable construction.
Crane and Heavy Lifting Operations: Sensors, including load cells, are frequently integrated into cranes, hoists, and lifting equipment to accurately measure the loads being lifted. This enables operators to ensure that the weight being lifted is within safe operating limits, preventing overloading and potential accidents.
Foundation Load Testing: Utilized in foundation load testing, load cells help to assess the bearing capacity and settlement behavior of foundations. They help determine the maximum loads that can be supported by the foundation, ensuring its stability and preventing settlement-related issues.
Structural Monitoring: Structural and civil engineers use load cells for ongoing monitoring of loads in structures such as tunnels, dams, and retaining walls. They provide continuous data on the loads acting on these structures, helping engineers assess their performance, detect any excessive stress or deformations, and ensure their long-term safety.
Material Testing: The materials used in construction range from steel to wood, even fabricated materials like rubber and foam. Load cells are employed in material testing laboratories to measure the strength and mechanical properties of construction materials such as concrete, steel, and timber. They play a critical role in conducting compression, tension, and bending tests, providing accurate load measurements for material performance evaluation.
Construction Equipment Calibration: As with all critical sensors, load cells are needed to calibrate and verify the accuracy of construction equipment, including weighing scales, hydraulic systems, and lifting devices. This ensures that the equipment operates correctly and delivers precise load measurements during construction activities. Utilizing Interface calibration grade load cells and systems is highly recommended for this type of use.
Construction Brochure
Interface and Infrastructure Markets Form a Perfect Partnership
/in Blog /by Jamie GlassInfrastructure projects are growing, as investment continues to climb for projects related to rebuilding, renewing and innovating applications in this sector. These global investments come from public and private organizations as demands to address roads, bridges, water supplies, transportation, energy […]
Infrastructure Industry Relies on Interface Force Measurement
/in Blog /by Jamie GlassThe safety and stability of the structures and facilities that are used by towns, cities, organizations, governments and countries are essential to their successful operations. In the design and construction, it is a requirement to ensure that every component measures […]
Where to Find 50 New Force Measurement Application Notes
/in Blog /by Jamie GlassOne of the advantages we have at Interface is that our application engineers and solutions experts are constantly recommending Interface load cells, torque transducers, instrumentation and accessories for a wide range of projects and programs. In this fortunate position, it […]
Interface’s Steering Role in All Types of Transportation
/in Blog /by Jamie GlassInterface serves a wide variety of industries that design and manufacture movers of people and objects. The transportation sector consists of companies that assist in the movement people or goods, as well as supporting infrastructure. Whether it is automobiles or […]
Interface Solutions Designed for Infrastructure Challenges
/in Blog /by Brian JohnsonAll infrastructure, big and small, needs to be designed with safety and durability in mind. Take for instance the massive amount of design, engineering and quality control that goes into a suspension bridge requires testing before and after it’s built. […]
Interface Crane Use Cases and Application Notes
/in Blog /by Brian JohnsonManufacturers and engineers of heavy equipment are rigorous about the design quality, performance and most importantly preserving safety. Having tools to test and monitor this type of equipment allows equipment producers and users to review performance at all stages, ultimately […]
Interface’s Sustaining Role in Arizona and the Global Business Ecosystem During COVID-19
/in Blog /by Brian JohnsonFor more than half a century, Interface has had the privilege of serving a wide variety of industries and helping our customers test, design, and manufacture products and infrastructure essential to everyday life. Our purpose at Interface defines our commitment […]
Seismic Application for Interface Load Pins
/in Blog /by Brian JohnsonThe range of applications of force measurement is wide-ranging across many industries. You can find Interface Mini Load Cells are frequently used to measure minute forces in precision medical devices, while our jumbo precision load cells that are rated for 2,000,000 […]