Additive manufacturing, known as 3D printing, has developed and grown since its first prototypes for 3-dimensional printing in the 1980s. By the early 2000s, additive manufacturing was beginning to create functional products.
Today, additive manufacturing has improved and continues to expand in creating objects like small-scale models, prototypes, and even full-scale manufactured parts and products. Its popularity is driven by less process time and a much cheaper cost for production.
Additive manufacturing is a layer-by-layer process used to create objects, molds, or prototypes. Various materials, including polymers, metals, ceramics, foams, gels, and biomaterials, can be used. In contrast to traditional manufacturing, additive manufacturing can create complex shapes and small sizes. Interface load cells play a crucial role in this process, measuring the force or weight during dimensional printing to ensure precision and quality control.
Force Measurement Additive Manufacturing Applications
- Monitoring Nozzle Forces
- In-Situ Force Controls
- Tension and Compression Durability Tests
- Characterizing Mechanical Properties
- Calibrating Robotic Arms
- Material Yield, Strength, Stress and Strain Testing
- Equipment Maintenance Systems for Nozzle Blockage
- Machine Quality Checks
- Machining and Part Finishing
- Prosthetic Prototyping
- 4D Equipment Design
Sensor Technology Benefits in Additive Manufacturing Use Cases
Process Monitoring: Interface Mini load cells are used in additive manufacturing for process monitoring. These load cells can be integrated into 3D printers to monitor the forces exerted during printing. By measuring the force applied by the print head or the build platform, manufacturers can ensure that the printing process is proceeding as expected and detect any anomalies that may affect the quality of the final product.
Specification Quality Control: Load cells are ideal for verifying the mechanical properties of the printed parts. By subjecting the printed objects to controlled mechanical tests, such as tensile or compression tests, manufacturers can determine whether the parts meet the required specifications and standards.
Material Testing: Interface sensor technologies are commonly used to test the materials prior to the actual printing process. By measuring the forces required to extrude or deposit the material during the creation process. Manufacturers can evaluate the strength, flexibility, and viscosity of the material, thus achieving a consistent print quality.
Structural and Prototype Testing: Product designers and engineers use load cells and multi-axis sensors to gather critical measurement data in testing the final prototype or structure of objects being printed, ensuring structural integrity. Manufacturers can determine and assess different factors, such as stiffness, strength, and durability, of the prototype to ensure it meets the required performance criteria.
Interface offers a variety of sensors for use in additive manufacturing processes, including:
- LBM Compression Load Button Load Cells
- Load Pins
- LW General Purpose Load Washer Load Cells
- LWCF Clamping Force Load Cells
- S-Type Miniature Load Cells
- MB Miniature Beam Load Cell
- BMI Overload Protected Miniature Beam Load Cell
- MTFS Miniature Tension Force Load Cell
- REC Road End Load Cell
- ULC Ultra Low Capacity Load Cell
- WMC Sealed Stainless Steel Miniature Load Cell
The range of sensors is especially important for industries that need precision data and easy integration into equipment and testing. These include industries that are turning to additive manufacturing, such as aerospace, medical, and automotive. Selecting the right load cell is critical to product development, and manufacturers rely on Interface due to the accuracy and reliability of our solutions.
AdditiveManufacturing_InfographicPoster
Interface Helps to Move Agriculture Innovation Forward
/in Blog /by Brian JohnsonThe agriculture industry is the backbone of most economies, as food production and farming are essential to everyone’s existence around the world. Advancements and innovations in this market are core to growing a sustainable food supply as well as for […]
Faces of Interface Featuring Garland Hawkins
/in Forceleaders /by Brian JohnsonFaces of Interface is an important series because it highlights the talented team members that keep Interface going strong. In this new ForceLeaders feature, we interviewed Garland Hawkins, our production planner for Interface’s most popular LowProfile load cells. A key […]
Faces of Interface Featuring Tim Matteson
/in Forceleaders /by Brian JohnsonThe Faces of Interface is an important series for the Interface IQ Blog because it highlights the talented people that keep Interface going strong. In this new ForceLeaders feature we interviewed Tim Matteson, product quality and improvement engineer for our […]
Interface Partners with Manufacturing Representative Firm GenTek
/in Blog /by Brian JohnsonIn a move that enhances its ability to expand premium force measurement solutions to a growing number of customers in the Southeast, Interface today announced a new partnership with manufacturer’s representatives GenTek Inc. GenTek focuses on providing technology solutions to […]
Interface Differentiator is Proprietary Strain Gage Manufacturing
/in Blog /by Brian JohnsonInterface products have been heralded for their accuracy, reliability, and quality for more than 50 years. We credit our vertically integrated approach to manufacturing as the most significant factor in our development of industry-leading force measurement products, meaning we control […]
Interface is a Critical Solutions Provider for OEMs
/in Blog /by Brian JohnsonThe hardware industry is rapidly making its way into taking advantage of the Industry 4.0 and Big Data eras. The idea that data insight can cut costs, increase efficiency and reduce downtime is spreading like wildfire throughout major OEMs (original […]
Interface Solutions for Industrial Markets
/in Blog /by Brian JohnsonThe industrial market is vast. The industry classification covers everything from manufacturing and assembly to mining and agriculture. The highly regulated environments involved in industrial applications often require advanced equipment and technologies for product design and development, as well as […]
Test Stand Applications for Force and Torque
/in Blog /by Brian JohnsonTest stands are essential equipment for manufacturers and testing engineers in the world of test and measurement. The test stand provides various testing products in a single “cabinet-like” structure. These systems have been used for a long time to gather […]
Celebrating Independence and American Manufacturing
/in Blog /by Brian JohnsonAs we celebrate Independence Day 2020 at Interface, we are also celebrating our history as an American manufacturer. We are a company founded in 1968 that started with a vision to engineer and build precision and quality products made in […]
Envisioning the Future of Force Measurement
/in Blog /by Brian JohnsonIt is estimated that the force measurement sensor industry market, which includes strain gages and load cells, is valued at $2 billion annually. This is a result of the diverse amount of application uses for these types of sensors, whether […]