Solution
Linear Test Stand
Customer would like to crush test a specimen in their linear stand. The customer would like to use force to determine when the deformation actually occurs.
Customer would like to crush test a specimen in their linear stand. The customer would like to use force to determine when the deformation actually occurs.
Interface provided Model 1210 Precision LowProfile® Load Cell with internal amplification of 0-10VDC Output.
Amplified Model 1210 Precision LowProfile® Load Cell was installed into the load string of the customer’s load frame and the scaled analog output from the load cell was connected to the customer’s instrumentation. When the force levels reached the crushing point, the customer’s software was able to read the output of the amplified load cell and record the value.
Notifications