Solution
Metal Press Cutting Machine
A customer wants to test the amount of force it takes to cut through different thickness’s of metal on their metal press cutting machine.
A customer wants to test the amount of force it takes to cut through different thickness’s of metal on their metal press cutting machine. They want to ensure their metal press cutting machine is working properly, and also its maximum limitation.
Interface’s suggests installing their 3AXX 3-Axis Force Load Cell underneath the plate where pieces of metal are placed to be cut, or punched holes in. When connected to the BX8-HD44 BlueDAQ Series Data Acquisition System, the force results of different metals being cut will be displayed, graphed, and recorded on the customer’s PC. It also has an analog output that can connect to the machines PLC in case of an overload.
The customer was able to determine the different amount of forces it took for their metal press cutting machine to cut through different types and thicknesses of metal.
Notifications