Solution
Water Bottle Dispensing and Weighing
A water bottle manufacturer wants to dispense and weigh the right amount of fluid into their bottles.
A water bottle manufacturer wants to dispense the right amount of fluid into their bottles, and then weigh the water bottles to ensure it is at the labeled weight on their product packaging. This is both to minimize waste, but also to meet the standard requirements.
Interface suggests using the MBP Miniature Beam Load Cell, and attaching it under a plate or platform the water bottle is placed on while it is being filled with fluids. The force weight is measured by the MBP Miniature Beam Load Cell, and connected to the 9870 High Speed High Performance TEDS Ready Indicator where results are captures, displayed, and can be recorded by the customer based on their needs.
The water bottle manufacturer received high accurate results of each water bottle being weighed in real time.