Testing the Reins
Think of nearly any piece of hardware, especially those with moving components, and chances are a force measurement device was used in its development and testing.
Interface supplies load cells, torque transducers, load pins, tension links, and data acquisition devices utilized in testing hardware components for automobiles, drones, rocket engines, medical devices, bridges, watercraft, and everything in-between including for horses.
The applications for our products grow broader every year, so much so that we are rarely surprised with the ingenuity and innovation abound. There are no limitations, including in the equipment utilized in core agriculture markets, which comprises of products used in the equine industry.
In one customer’s project, were able to provide valuable sensor technology for a test and measurement project for products used with horses. Included below is a brief preview of the two new applications notes we developed based on the specific requirements for this equine industry design.
A customer came to Interface needing to quantify the poll pressure on the bridle of a horse. We created a solution using both a Wireless Telemetry System (WTS) and a Bluetooth® Telemetry System (BTS) Equine Bridle Tension System, with two SMA Miniature S-Type Load Cells in both the line of the reins and that of the cheekpiece on one side of the horse to study the dynamic response of the cheekpiece tension to rein tension in the ridden horse. Utilizing the WTS or BTS, the valuable data can be displayed and recorded in real time.
Within the real experimental system these sensors were used to test the tension resulting from the rider’s hands, the horse’s mouth and the bit, the elasticity of the equine mouth provides a “floating” fulcrum and a potential source of time-lag and decoherence between the dynamic rein and cheekpiece tensions. Because the cheekpiece is directly attached to the headpiece, we we’re able to assume that forces seen in the cheekpiece are those that are applied to the poll of the horse.
Want to learn more about this agriculture industry solution? Be sure to read the Equine Industry WTS and BTS Bridle Tension System application notes.