Torque Transducers and Couplings are the Perfect Pairing

Torque transducers require couplings to enhance precision and reliability in performance. The pairing ensures accurate measurements. The coupling enables the torque transducer to precisely measure torque while maintaining a secure mechanical connection to the rotating components. This facilitates data collection, analysis, and control, leading to improved performance, efficiency, and reliability when using a torque transducer in various test and measurement applications.

Couplings are designed to provide a strong and secure connection between the shafts, ensuring efficient torque transmission while minimizing stress and wear on the components. They come in distinct types and designs, each suited for specific applications and operating conditions.

For example, rigid couplings provide a solid and inflexible connection between the shafts, allowing for precise torque transmission but offering little or no flexibility to compensate for misalignments. Whereas flexible couplings are designed to accommodate small misalignments and angular offsets between the shafts. They use flexible discs to provide some degree of flexibility, dampen vibrations, and reduce stress on the connected components.

Interface Torque Transducer Models T2, T3, T4, T5, T6, T7, T8, T11 and T25 offer a range of product-specific coupling options. It is important to note that couplings are not universal, and your best options are always the couplings designed for the specific model, thus the perfect pairing. To demonstrate the range of options, here is a quick list of coupling designs:

  • Floating Mount Keyed Single Flex Couplings
  • Pedestal or Foot Mount Keyed Double Flex Couplings
  • Floating Mount Clamping Ring Single Flex Couplings
  • Pedestal or Foot Mount Clamping Ring Double Flex Couplings
  • Floating Mount Shrink Disk Single Flex Couplings
  • Pedestal or FootMount Shrink Disk Double Flex Couplings
  • Floating Mount Single Flex Couplings
  • Pedestal or Foot Mount Double Flex Couplings

A torque transducer coupling is a specific coupling designed to facilitate the connection and torque measurement between a torque transducer and a rotating shaft, providing accurate and reliable torque data. Whenever you are selecting an Interface torque transducer, be sure to request or add the Interface couplings that are designed for that specific transducer model. It is especially important to review the couplings features that pairs with your specific transducer. They are designed to work together, and you risk any problems or potential transducer failure.

Torque Transducers Require Couplings for Accuracy and to Safeguard Your Investment

Without a coupling, the torque transducer cannot be mechanically connected to the rotating shaft or component. As a result, it will not be able to measure the torque being transmitted through the shaft. This means you will lose the ability to accurately monitor and analyze torque in the system.

Using couplings is a standard requirement when using a torque transducer. They provide the mechanical connection, transmission and reduce misalignments, which all contributes to accurate and reliable torque measurements with torque transducers.

A coupling provides a means of mechanically connecting the torque transducer to the rotating shaft or component from which torque is being measured. It ensures a secure and reliable connection between the transducer and the system under test. In the absence of a coupling, the torque transducer may not be securely attached to the rotating shaft. This can lead to relative movement or slippage between the transducer and the shaft,

The coupling enables the transfer of torque from the rotating shaft to the torque transducer. As the shaft rotates, the torque is transmitted through the coupling to the transducer, which measures and converts it into an electrical signal for further analysis or control.

A coupling helps to compensate for small misalignments between the shaft and the transducer. Without a coupling, any misalignment between the two components can put additional stress on the transducer and the shaft, potentially causing premature wear, increased friction, or even catastrophic failure.

Couplings can also provide vibration damping properties by design, as they absorb or dampen vibrations and shocks that may be present in the system. This helps to protect the torque transducer from excessive mechanical stresses and safeguards torque measurements. Without a proper coupling, the transducer may also be susceptible to excessive vibrations or shocks, increasing the risk of mechanical failure.

Torque Transducer and Couplings Applications

If you are looking at a torque transducer use case, assume there are couplings that are part of the application. To point out common examples of testing programs that utilize couplings with high-performance torque transducers, the first place to start is in the automotive industry. In the automotive industry, high-performance torque transducers with couplings are used for various testing purposes. For example, during the development and testing of engines, transmissions, and drivetrain components, torque transducers coupled with the rotating shafts allow for precise measurement of torque and power output. Torque measurement data is crucial for performance analysis, efficiency optimization, and durability testing.

Torque transducers with couplings are extensively utilized in the engineering, testing, and use of industrial automation, machinery and equipment. Manufacturing processes that involve rotating components, such as pumps, compressors, and turbines, are using torque transducers coupled with the shafts to provide measurements of torque. Accuracy in data helps monitor the efficiency of the machinery, detect deviations, and ensure standard operation. All of this contributes to preventative maintenance.

There are many R&D use cases where torque transducers with couplings are required. We often see torque transducers and couplings used in material testing and structural analysis. In the renewable energy sector, wind turbines and hydroelectric generators use torque transducers and couplings.

These examples the coupling enables the torque transducer to accurately measure torque while maintaining a secure mechanical connection to the rotating components.  To explore more about couplings, be sure to tune into our recorded torque transducers webinar.


Additional Resources

Couplings 101

Torque Transducer Selection Guide

Miniature Torque Transducers 101

Choosing the Right Torque Transducer

Fuel Pump Optimization & Rotary Torque

A Comparison of Torque Measurement Systems White Paper

Rover Wheel Torque Monitoring

Torque Measurement Primer